Metals and Alloys and Their Properties
Use the chart below to find the
chemical element symbol,
specific gravity,
melting point,
IACS rating, or
density
of various metals and alloys.
| Metal/Alloy |
Symbol |
Specific Gravity |
Melting Point: °C |
Melting Point: °F |
IACS Rating |
Density (lb/in3) |
| Aluminum |
Al |
2.71 |
660 |
1,220 |
64.90 |
0.0978 |
| Antimony |
Sb |
6.62 |
630 |
1,167 |
4.42 |
0.2390 |
| Arsenic |
As |
5.73 |
817 |
1,502 |
4.90 |
0.2070 |
| Beryllium |
Be |
1.83 |
1,280 |
2,336 |
9.32 |
0.0660 |
| Bismuth |
Bi |
9.80 |
271 |
520 |
1.50 |
0.3540 |
| Brass (70‑30) |
-- |
8.51 |
900 |
1,652 |
28 |
0.3070 |
| Bronze (5% Sn) |
-- |
8.87 |
1,000 |
1,382 |
18 |
0.3200 |
| Cadmium |
Cd |
8.65 |
321 |
610 |
22.70 |
0.3120 |
| Calcium |
Ca |
1.55 |
850 |
1,562 |
50.10 |
0.0560 |
| Cobalt |
Co |
8.90 |
1,495 |
2,723 |
17.80 |
0.3210 |
| Copper |
Cu |
8.95 |
1,085 |
1,984 |
100 |
0.3240 |
| Copper‑Rolled |
-- |
8.89 |
1,083 |
1,981 |
100 |
0.3210 |
| Copper‑Tubing |
-- |
8.89 |
1,083 |
1,981 |
100 |
0.3210 |
| Gold |
Au |
19.30 |
1,063 |
1,945 |
71.20 |
0.6970 |
| Graphite |
-- |
2.25 |
3,500 |
6,332 |
0.22 |
0.0812 |
| Indium |
In |
7.30 |
156 |
311 |
20.60 |
0.2640 |
| Iridium |
Ir |
22.40 |
2,450 |
4,442 |
32.50 |
0.8090 |
| Iron |
Fe |
7.20 |
1,200-1,400 |
2,192-2,552 |
17.60 |
0.2600 |
| Iron‑Malleable |
-- |
7.20 |
1,500-1,600 |
2,732-2,912 |
10 |
0.2600 |
| Iron‑Wrought |
-- |
7.70 |
1,500-1,600 |
2,732-2,912 |
10 |
0.2780 |
| Lead |
Pb |
11.40 |
327 |
621 |
8.35 |
0.4120 |
| Magnesium |
Mg |
1.74 |
651 |
1,204 |
38.70 |
0.0628 |
| Manganese |
Mn |
7.20 |
1,245 |
2,273 |
0.90 |
0.2600 |
| Mercury |
Hg |
13.65 |
-38.90 |
-37.70 |
1.80 |
0.4930 |
| Molybdenum |
Mo |
10.20 |
2,620 |
4,748 |
36.10 |
0.3680 |
| Monel (63‑37) |
-- |
8.87 |
1,300 |
2,372 |
3 |
0.3200 |
| Nickel |
Ni |
8.90 |
1,452 |
2,646 |
25 |
0.3210 |
| Phosphorus |
P |
1.82 |
44.10 |
111.40 |
10-17 |
0.0657 |
| Platinum |
Pt |
21.46 |
1,773 |
3,221 |
17.50 |
0.7750 |
| Potassium |
K |
0.86 |
62.30 |
144.10 |
28 |
0.0310 |
| Selenium |
Se |
4.81 |
220 |
428 |
14.40 |
0.1740 |
| Silicon |
Si |
2.40 |
1,420 |
2,588 |
10-5 |
0.0866 |
| Silver |
Ag |
10.50 |
960 |
1,760 |
106 |
0.3790 |
| Steel (Carbon) |
-- |
7.84 |
1,330-1,380 |
2,436-2,516 |
10 |
0.2830 |
| Stainless (18‑8) |
-- |
7.92 |
1,500 |
2,732 |
2.50 |
0.2860 |
| Stainless (13‑Cr) |
-- |
7.78 |
1,520 |
2,768 |
3.50 |
0.2810 |
| Stainless (18‑Cr) |
-- |
7.73 |
1,500 |
2,732 |
3 |
0.2790 |
| Tantalum |
Ta |
16.60 |
2,900 |
5,414 |
13.90 |
0.5990 |
| Tellurium |
Te |
6.20 |
450 |
846 |
10-5 |
0.2240 |
| Thorium |
Th |
11.70 |
1,845 |
3,353 |
9.10 |
0.4420 |
| Tin |
Sn |
7.30 |
232 |
449 |
15 |
0.2640 |
| Titanium |
Ti |
4.50 |
1,800 |
3,272 |
2.10 |
0.1620 |
| Tungsten |
W |
19.30 |
3,422 |
6,192 |
31.50 |
0.6970 |
| Uranium |
U |
18.70 |
1,130 |
2,066 |
2.80 |
0.6750 |
| Vanadium |
V |
5.96 |
1,710 |
3,110 |
6.63 |
0.2150 |
| Zinc |
Zn |
7.14 |
419 |
786 |
29.10 |
0.2580 |
| Zirconium |
Zr |
6.40 |
1,700 |
3,092 |
4.20 |
0.2310 |
How is the Chemical Element Symbol or Metal Abbreviation Determined?
Chemical element symbols or abbreviations for metals are typically one or two letters from the element's Latin name
or a shortened English version of the name of the metal.
- Sb for Antimony (from the Latin word Stibium)
- Au for Gold (from the Latin word Aurum)
- Cu for Copper (from the Latin word Cuprum)
- Fe for Iron (from the Latin word Ferrum)
- Pb for Lead (from the Latin word Plumbum)
- Hg for Mercury (from the Latin word Hydrargyrum, which means "silver water")
- K for Potassium (from Kalium, Arabic for "plant ashes")
- Ag for Silver (from the Latin word Argentum, which means "shiny, white")
- Sn for Tin (from the Latin word Stannum)
- W for Tungsten (from the German word Wolfram)
What is Specific Gravity?
Specific gravity, also known as relative density, is a way to compare the
density of a metal to the density of water at 4°C.
A specific gravity greater than 1 indicates the metal is denser than water at 4°C, while a value less than 1 means it's less dense.
What is the Melting Point of a Metal?
The melting point of a metal is the temperature at which it transitions from a solid state to a liquid state.
What is an IACS Rating?
The International Annealed Copper Standard (IACS) rating is the percentage of conductivity of a metal or alloy relative to copper.
The density of a metal refers to its mass per unit volume. In simpler terms, it tells you how heavy a specific
amount of that metal is compared to its size.
The higher the density, the heavier the metal will be for its size.
See Our Other Helpful Guides:
WARNING: For safety, call a licensed electrician or consult the NEC®. All licensed electricians have passed examinations
covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.