Add More Items
View All Quick Selects
These conduit fill charts are used to determine how many compacted conductor wires can be safely run through non-PVC conduit tubing or pipe. Compacted wire is also called compact stranded wire or compressed wire. This page includes two conduit fill tables: one for compact THHN wire, and one for compact XHHW wire. In each conduit fill chart, each row (going across) shows different conduit sizes and types: either Electrical Metal Tubing (EMT), Intermediate Metal Conduit (IMC), or Galvanized Rigid Steel Pipe (Rigid metal conduit, RMC). Each column (going up and down) is a different gauge of wire, either AWG or MCM. The results show the allowable number of wires for each size/type of conduit and compacted or compressed wire, whether aluminum, copper, or another conductor material, based on the 2020 NEC® code.
Not looking for compact wire guides? See our other conduit fill guides: PVC Conduit Fill Chart , Metallic Conduit Fill Chart , and ENT Conduit Fill Chart .
Compacted or compressed stranding is a configuration with concentric strands (typically aluminum but not always) in which each layer is passed through a compacting die and compressed to reduce the total conductor diameter size by approximately ten percent. This means compacted conductors can provide more conduction, literally more strands of wire, in the same size or even smaller size of conduit.
↑ To Top
This page contains two separate conduit fill charts, one for compacted THHN wire and one for compacted XHHW wire. Choose a wire type below, THHN or XHHW, then you will be able to drill down to a specific size.
To jump to the section of the Conduit Fill Chart for your gauge of compacted THHN wire, select a wire size.
To jump to the section of the Conduit Fill Chart for your gauge of compacted XHHW wire, select a wire size.
Above information referenced from Table C.1(A), Table C.4(A), and Table C.9(A) in the 2020 NEC® (National Electric Code®).
For more information on filling the following types of conduit with compacted conductors, please see the tables listed below in the Appendix C of the National Electric Code® (NEC®) of 2020.
Electrical Non-Metallic Tubing (ENT) -- Table C.2(A) Flexible Metal Conduit (FMC) -- Table C.3(A) Liquidtight Flexible Non-Metallic Conduit (Type LFNC-A) -- Table C.5(A) Liquidtight Flexible Non-Metallic Conduit (Type LFNC-B) -- Table C.6(A) Liquidtight Flexible Non-Metallic Conduit (Type LFNC-C) -- Table C.7(A) Liquidtight Flexible Metallic Conduit (LFMC) -- Table C.8(A) Rigid PVC Conduit, Schedule 80 -- Table C.10(A) Rigid PVC Conduit, Schedule 40 -- Table C.11(A) Type A PVC Conduit -- Table C.12(A) Type EB PVC Conduit -- Table C.13(A)
If you have any other questions see the NEC® Code Book or ask an Elliott Electric Salesperson.
Shop Wire & Cable
Shop Conduit
Shop Fish Tape
Warning: When using this information to perform electrical work, call a licensed electrician and consult the NEC® for safety. All licensed electricians have passed examinations covering the National Electric Code®, know state and local building codes, and may carry insurance to cover damages.