Job Description:
Shifts Available: Day Shitt: 5:300am - 2:30pm or until route is complete.
At Elliott Electric Supply, people come first. We’re a team that values respect, hard work, and collaboration. When you join Elliott, you’re not just taking a job-you’re building a career with a company that invests in its people.
Support warehouse operations by transporting materials over designated routes; ensuring safe operation of vehicles. Provide excellent customer service by making prompt and courteous deliveries of orders. Ensure that material loaded on the truck is as listed on the Ship Ticket and Delivery Manifest and is secured for safe transport from store to destination. Unload materials for customers at each delivery location in an orderly fashion while verifying that material is correct based on the Ship Ticket. Perform daily detailed inspection of vehicle to ensure general maintenance and safety of vehicle. This is a safety-sensitive position, the ability to work in a constant state of awareness and in a safe manner is imperative.
Qualifications:
High school diploma or equivalent preferred. Valid Driver's License in state of residence with 3 years driving history. Acceptable Motor Vehicle Record with no type A violation; or no more than (1) type B violation in past (3) years. A minimum of 1 year of driving experience within the past 36 months, operating a commercial motor vehicle with a gross vehicle weight rating (GVWR) of 10,001 lbs. or more preferred. Read, comprehend, write, perform calculations, input accurately, reason, and analyze. Function independently, completing various tasks accurately with close attention to detail.
Physical Requirements: Frequent driving is required in all types of weather conditions. Must adhere to the proper safety regulations since there will be occasional exposure to events such as excessive noise and moving machinery. Frequently walk, bend, squat, climb, kneel, pushing, pulling, and reaching. Regular handling of objects and lifting of up to 75 pounds. Physically qualified to drive a motor vehicle by the medical qualification standards in Sec. 391.41. A Department of Transportation physical exam will be conducted by a licensed medical examiner. The USDOT's Drug and Alcohol Testing Regulation, 49 CFR Part 40, at 40.151(e), does not authorize 'medical marijuana' under state law as a valid medical explanation for a transportation employee's positive drug test result. Must have an Active CDL Class A Driver's License.
Job Type: Full-Time
Contact:
Tammie Henderson (972)206-0016
Location: Farmers Branch, TX (DFW RDC - 34)
Apply For This Position